Can an Altivar drives be mounted horizontally?

Article available in these languages: Tiếng Tây Ban Nha

Issue:
Wants to mount his Altivar Drive horizontally.

Product Line:
Altivar Drive

Environment:
All serial numbers for Altivar Drive

Cause:
N/A

Resolution:
No the Altivar Drives cannot be mounted horizontally. The drives should be installed vertically at ± 10°.
Please refer to you drives installation manual for proper mounting conditions.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: