What version of Unity Pro will run on Windows 10?

Issue
At what release did Unity Pro begin supporting Windows 10?

Product line
Unity Pro, Control Expert

Resolution
Windows 10 OS support began with Unity Pro V11.0 which supports:
- Windows 7 32&64 bits
- Windows 8.1 32&64 bits
- Windows 10 32&64 bits
- Windows Server 2012

as of 7/1/2022 the latest Unity Pro version release has been renamed and is now EcoStruxure Control Expert V15.1 which supports:
-  Microsoft Windows 7 Professional edition 32/64 bits SP1
-  Microsoft Windows 10 32/64 bits
-  Microsoft Windows Server 2016
NOTE: An operating system Windows 64 bits is mandatory for projects with Modicon M580 controller, or projects using DTMs.
Unity Pro is now called EcoStruxure Control Expert starting at version14.0


Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: