What is the cable to use to connect the HMIGTO to the Premium PLC on the TER port for Unitelway?
Issue:
What is the cable to use to connect the HMIGTO to the Premium PLC on the TER port for Unitelway?

Product Line:
Magelis HMI (XBTGT, XBTGK, HMISTO, HMISTU, HMIGTO, HMIGTU, XBTGH)

Resolution:
The cable to use would be the XBTZ9780 in order to connect the HMIGTO/XBTGT/HMIGTU/HMISTU/HMISTO to the TSX Premium series PLC via the TER port to communciate over Uni-Telway protocol.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: