Can I use SoMove software on a ATV28 drive (also ATV16, ATV18, ATV11, ATV56, ATV66)?
Issue:
Using SoMove software on a ATV28 drive (also ATV16, ATV18, ATV11, ATV56, ATV66).

Product line:
ATV28, ATV16, ATV18, ATV11, ATV56, ATV66

Environment:
SoMove

Cause:
n/a

Resolution:
No, SoMove will not work with ATV28 drives or any of these other, obsolete products.

We do not offer a software package for these old, discontinued and obsolete drives.

Schneider Electric Việt Nam

Tìm hiểu thêm
Danh mục:
Bài viết có thể hữu ích
Tìm hiểu thêm
Danh mục: