What licenses are required for PowerSCADA Anywhere in PSO 8.1 and above?
Issue
User wants to confirm what licensing is required to implement PowerSCADA Anywhere

Product
PowerSCADA Operation 8.1
PowerSCADA Operation 8.2
PowerSCADA Operation 9.0

Environment
PowerSCADA Operation Remote Client

Cause
Documentation includes some data or conflicting data regarding what licensing is required for PowerSCADA Anywhere

Resolution
In order to implement PowerSCADA Anywhere, 3 separate license components are needed
1) PowerSCADA Anywhere Client License (5 seats per license)
2) PowerSCADA Operation client license, 1 per desired seat (either control or view-only)
3) Microsoft Client Access License, 1 per desired seat

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: