How is a dynamic braking resistor added to an ATV32 drive?

Article available in these languages: Tiếng Tây Ban Nha

Issue:
Addition of dynamic braking resistor on ATV32.

Product Line:
Altivar 32

Environment:
All

Cause:
N/A

Resolution:
Wiring:
The resistor should be wired to the PA and PB terminals on the drive.

Programming:
DRI- > CONF > FULL > FUN- > STT
Go into CONF menu, then FULL menu, then FUN menu.
Under FUN, go into STT- menu.
Set brA to [No].

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: