Is it possible to downgrade the Vijeo Designer Runtime on a Magelis Advance Panels?
Issue:
Is it possible to downgrade the Vijeo Designer Runtime on Magelis Advance Panels?

Product Line:
Magelis XBTGK/GT/GC, HMISTU/STO/GTO/G3U

Resolution:
Yes, it is possible to downgrade the runtime by downloading to filesystem on a CF card, SD card or USB flash drive (depending on which target you have).\

Please refer to this FAQ on how to perform a filesystem download to downgrade the runtime version:
https://www.se.com/ww/en/faqs/FA199001/

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: