Is the ENA (Pumpjack, Walking Beam pump) function available in the process drive?
ISSUE:
Availablity of ENA function (Pumpjack, Walking Beam Pump) in the Altivar Process Drives.

Product Line:
ATV600, ATV900 series

Environment:
All Models, All Serial Numbers

Cause:
Information unavailable in current literature.

Resolution:
The ENA function is not available in the ATV600 series process drives but is available in the ATV900 series process drives.
Please refer to the programming manual for the ATV900 series for further details.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: