Why will my Altivar Drive not accept any program changes?
Issue:
Drive not accepting program changes

Product Line:
ATV12, ATV312, ATV61,ATV71, ATV312, ATV32

Environment:
All

Cause:
Unable to assign drive parameters, Drive will not accept changes.

Resolution:
Typical reasons that a VFD will not allow a parameter to be changed:
Verify the drive does not have an active run command.  Most parameters changes require the VFD to not be in run status.
Verify the parameter is not incompatible with other parameter settings.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: