Can programs created with Modsoft be opened with the ProWORX 32 software?
Issue
Open Modsoft project with ProWORX 32

Product Line
ProWORX 32

Resolution
Yes. Programs created with Modsoft can be imported, then opened, using ProWORX 32 software. With the ProWORX 32 software up and running, go to <FILE> then <IMPORT DATABASE>, select File Type as (*.CFG) for Modsoft, then go into the folder that has the Modsoft *.CFG file and select it, click on the <OPEN> button and the conversion process will begin.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: