Can the M580 PLC be started remotely?
A discrete input can be configured to the M580 from Run/Stop mode.
  • Set %Ir.m.c to 1: The M580 switches to Run mode (execute the program).
  • Set %lr.m.c to 0: The M580 switches to Stop mode (stop program execution).
    NOTE: A Stop command takes priority over a Run command. A Stop command sent from a terminal or via the network has priority over the %lr.m.c input.
    An error detected on the Run/Stop input causes the M580 to switch to Stop mode.
    Do not activate this option if the associated discrete input is mapped in state RAM because this inhibits the start-up of the M580.
    Managing Run/Stop Remote Access
    When configuring the M580 CPU, you can help prevent remote commands/requests from accessing the CPU Run/Stop modes.
    Select the respective Run/Stop input and Run/Stop by input only check boxes according to the following table parameters to
    determine the type of remote access for your system.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: