Vijeo Designer cannot run simulation. Error: "Could not start runtime. Make sure runtime is installed."
Issue:
Unable to launch the Vijeo Designer simulation mode.

Product Line:
Vijeo Designer (all versions)

Resolution:
One possible cause for this error is if there is a file or folder at C:\ named "Program". Typically this file or folder is locked and cannot be deleted normally. If one exists, reboot your PC in safe mode to either rename it or delete it.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: