Can a SMD be programmed to display only specific circuits on a BCPM?
Issue:
When using a SMD to display measurements from a BCPM, a user would like to only display circuits that are in use.

Product Line:
BCPM
Sub Meter Display (SMD)

Environment:
Sub Meter Display configuration

Resolutions:
It is not possible to configure a SMD to display only specific circuits/channels from a BCPM.
All circuits (those in use and not in use) will be present when using a SMD to view measurements from a BCPM.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: