How to achieve the centralized security editor
Question:
How to achieve the centralized security editor in unity pro ?

Answer:
Attached  is information on how to configure a centralized Security Editor.
This procedure allows to configure Unity & Security Editor so that all PCs running Unity pro takes Security Editor configuration (user names, user rights, audit trail....) from a  unique location.

This has only been tested in combination with AutoSave.
It has not yet been validated in standalone with Unity Pro...eg : in such architecture, if comminucation is lost between server and PC, Unity will not start
If customer is using Autosave, please look into such solution in collaboration with MDT Software.

Schneider Electric Việt Nam

Phần đính kèm
Centralized security Database.zip [1.38 MB]
Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: