What’s the least version of TSXCUSBMBP driver to run on Win Server 2012 R2 64bit
Question:
what’s the least version of TSXCUSBMBP driver to run on Win Server 2012 R2 64bit?

Answer:
Windows Server 2012 R2 is based on the Windows 8.1 kernel. The v8.0 and v8.1 support both of these OS's.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: