If an application built for a lower level M580 HSBY CPU can be downloaded & executed in a higher level M580 HSBY CPU?

Article available in these languages: Tiếng Tây Ban Nha

Yes,an application built for the BMEH582040 is downloadable and executable on the BMEH584040, BMEH586040.
An application built for the BMEH584040 is downloadable and executable on the BMEH586040.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: