Where is the run command connected on the ATS01...FT?

Article available in these languages: Tiếng Tây Ban Nha

Issue:
How is the run command wired to the ATS01...FT Altistart Softstart?

Product Line:
ATS01

Environment:
ATS01...FT

Cause:
Wire diagram not clear

Resolution:
External control voltage must be used.
If 110-240Vac control voltage is used. (can use the line voltage in the line inputs)
CL1/0 (neutral) and CL2 (120Vac) must be applied at the same time as line voltage.
If +24Vdc control voltage is used .
CL1/0 (-) and 24V (+) must be applied at the same time as line voltage.
Refer to manual catalog part number 8637CT0401
NOTE:  A contactor or starter and overload protection are required with these softstarts.

Schneider Electric Việt Nam

Tìm hiểu thêm
Sản phẩm:
Bài viết có thể hữu ích
Tìm hiểu thêm
Sản phẩm: