What is Config ELEC?
Config ELEC is an application for Smartphone.
It is a tool used to configure the Wiserlink system with MIP or the Smartlink ELEC system
The configuration is a necessary step to ensure the proper functioning of your products/system.
In case of  WiserLink system, Config ELEC allows to:
- Make the pairing between MPR and MPE
- Set the pulse weight of the MPR and M2I
- Set alarms for M2I
In case of a Smartlink ELEC system, Config ELEC allows to:
- Configure and test the different inputs / outputs.

Schneider Electric Việt Nam