What are the part numbers for the remote keypad and mounting accessories for Altivar Process Drives?
Issue:
What are the part numbers for the remote keypad and mounting accessories for Altivar Process Drives?

Product Line:
Altivar Process Drives

Environment:
Keypad

Cause:
Remote mounting

Resolution:
The Altivar Process keypad is part number VW3A1111
keypad
The Door mounting kit (Type 12) for the keypad is VW3A1112
keypad2
Cable for remote mounting (1 meter)- VW3A1104R10
Cable for remote mounting (3 meter)- VW3A1104R30
Cable for remote mounting (5 meter)- VW3A1104R50
Cable for remote mounting (10 meter)- VW3A1104R100
keypad3

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: