Are fast screws sufficient to ensure the holding of the frame of my Resi9 Electrical Panel on Insulatin backpart?Yes, the screws supplied with the chassis are sufficient (installed according to the description in the manual) if you are using the Plus backpart
Đã phát hành cho:Schneider Electric Việt Nam