Can a 63.75" tall PDU be installed into a 38U NetShelter CX cabinet?
Issue:
The 63.75" tall PDU does not fit onto the accessory rail. Will it fit anywhere else inside the cabinet?

Product Line:
NetShelter CX

Environment:
AR4038A, AR4038IA

Cause:
One of the 63.75" tall PDUs has been specc'd into a 38U NetShelter CX cabinet.

Resolution:
Yes, the 63.75" tall PDUs can attach to the rear mounting rail. Please see the attached file for mounting instructions.

Schneider Electric Việt Nam

Phần đính kèm
20160729 Tall PDU Mounting Into 38U NetShelter CX.docx [5.95 MB]
Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: