What are the recommended wire sizes for the Altivar 600 Process Drive?

Article available in these languages: Tiếng Nhật

You would normally size the wire according to NEC and use a rating of 125% of the input line current for the rated drive.  See below for the wire size recommendation based on Frame size.

img1
f4-6
https://www.se.com/us/en/download/document/EAV64301/

“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: