What is the cable diameter supported by MF1 CT for phase current measurement?
The diameter of the cable should be less than 40 mm (< 40 mm) is supported by MF1 CT for phase current measurement.
The 40mm cable also should work but the positioning of cable should be correct else the performence may not be optimum.

Schneider Electric Việt Nam