PM8000 default SNMP register map
Issue
Want to know what values are linked to the SNMP Mapping module in the PM8000.

Product Line
PowerLogic PM8000 series meter

Environment
Advanced metering offer

Resolution
Simple Network Management Protocol (SNMP) is part of the Transmission Control Protocol/Internet Protocol (TCP/IP) protocol suite. It is an application layer protocol that facilitates the exchange of network management information between devices, allowing you to manage network performance and to identify and solve problems on networks with devices of various types.

PM8000 meter supports SNMP once SNMP is activated on the meter. The meter's MIB file needs to be upload into the NMS managing your meter. See FA276689 for more details about setting SNMP. The MIB file is included with the meter's Firmware ZIP file located on se.com.

*Warning: Changing your meter’s default SNMP configuration assumes that you have an advanced understanding of ION architecture, SNMP, and the communications network and power system that your meter is connected to.

Enabling SNMP provides SNMP access to the meter values linked to the SNMP Mapping module. You can configure the SNMP Mapping module to link to different meter values. By default, the following meter values are linked to the SNMP Mapping module:
I a kVAR tot Vll ca Vln avg Ib mean kW sd mx del-rec
I b kVA tot Vll avg Freq Ic mx kW sd del
I c PF sign tot Vln a Ia mx Ic mean kW sd rec
I avg Vll ab Vln b Ia mean kW sd mx del kW sd del-rec
kW tot Vll bc Vln c Ib mx kW sd mx rec kVAR sd mx del
kVAR sd mx rec kVAR sd mx del-rec kVAR sd del kVAR sd rec kVAR sd del-rec kVA sd mx del
kVA sd mx rec kVA sd mx del-rec kVA sd del kVA sd rec kVA sd del-rec kWh del
kWh rec kWh del-rec kVARh del kVARh rec kVARh del-rec kVAh del
kVAh rec kVAh del-rec

The following meter information is always provided by default and cannot be configured:
Voltsmode, Model number, Serial number, Device name, Firmware version, MIB version

Note: If you change your meter’s default values you must modify the default MIB file to reflect the new values.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: