How to install Vijeo Designer as Demo/Trial/Limited Edition mode

Article available in these languages: Tiếng Tây Ban Nha, Tiếng Thổ Nhĩ Kỳ

Issue
How does one install Vijeo Designer as Demo/Trial/Limited Edition mode?

Product Line
Vijeo Designer v6.2
Vijeo Designer v6.3

Environment
HMI Configuration software for Windows

Resolution

Vijeo Designer v6.2
There are three modes of installation for Vijeo Designer v6.2. They include:
1) Limited Edition mode - this allows full functionality of configuration, but only allows download to the HMISTO and HMISTU series HMIs
2) Trial mode - this allows full functionality and downloading to all HMI types, but is limited to 21 days from the install date
3) Fully licensed - this allows full functionality without time or download restriction

To Install in Limited Edition mode
When prompted from the installation wizard from the installation files, leave the Reference Number and Serial Number both blank.

To Install in Trial Mode:
When prompted from the installation wizard from the installation files, use:
Reference Number: VJDSNDTGSV62M
Serial Number: (any 11 numeric digits) 01234567890

To Install in Fully Licensed Mode:
When prompted from the installation wizard from the DVD / ISO, use the Reference Number and Serial Number provided with the purchased DVD or emailed license after purchase. Then launch the Vijeo Designer License Manager from "C:\ProgramData\Microsoft\Windows\Start Menu\Programs\Schneider Electric\Vijeo Designer 6.2\" -> License Manager shortcut and follow the instructions in the Wizard to register.


Vijeo Designer v6.3
Vijeo Designer v6.3 can only be installed in two modes:
1) Trial mode - this allows full functionality and downloading to all HMI types, but is limited to 42 days from the install date
2) Fully licensed - this allows full functionality without time or download restriction

To Install in Trial Mode:
Unlike Vijeo Designer v6.2, there will be no required prompt to enter the Reference Number or Serial Number. Simply installing the software as-is will give you a 42-day trial as soon as you launch the software.

To Install in Fully Licensed Mode
After you have installed the software, launch the "HMI License Manager" where you can enter the Activation ID (A-XXXX-XXXX-XXXX) to register the product.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: