Will the ATV320 be available above 5HP in 480V compact version?
Issue:
ATV320 availability above on 5HP in 480V compact version.

Product Line:
ATV320 series

Environment:
Compact version (C)

Cause:
Information unavailable or difficult to find in current literature.

Resolution:
The ATV320 series, 480V rating, will only be available up to 5HP in the compact (C) version.  Above 5HP, the Book (B) version will be available from 7.5HP to 20HP.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: