Does Schneider Electric offer motor type BDM4564S0115 ?
No, the motor type BDM4564S0115 is a customized version of Brushless DC motor which has special design features unique for the OEM machine builder that uses this model.

This model is proprietary for the OEM machine builder and the sale of this model is restricted to only the OEM.

Customers looking for BDM4564S0115 must contact the OEM machine builder to get spares.

rev 9-16-19

Schneider Electric Việt Nam

Tìm hiểu thêm
Sản phẩm:
Tìm hiểu thêm
Sản phẩm: