Is it possible to change the motor related timers of the Process Drive from seconds to minutes?
Issue:
Early versions of the ATV600 and ATV900 drives only displayed time in seconds

Product Line:
Process Drive

Environment:
All models and serial numbers

Cause:
None

Resolution:
For ATV600 series drives with firmware V2.4 and less and ATV900 V2.1 and lower, it is not possible to change the motor related timers from seconds to minutes.
For more recent versions the time is available in Days/Hours/Minutes/Seconds format.

You can view the current values and reset the timers in the Counter Management menu.

Counter management can be found in menu 4.9.
The following counters can be monitored:
[Motor Run Time] - rtH
[Power-on Time] - PtH
[Fan Operation Time] - FCPt

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: