How do I connect a EPO circuit to Smart-UPS VT or Galaxy 3500 Battery XR Frame?
Issue:
How do I connect a EPO circuit to Smart-UPS VT or Galaxy 3500 Battery XR Frame?


Product line:
Smart-UPS VT & Galaxy 3500 Battery XR frames


Environment:
All models/ All serial numbers


Cause:
How do I connect a EPO circuit to Smart-UPS VT or Galaxy 3500 Battery XR Frame?



Resolution:
See illustration below and attached file:

1
This means that you shall connect UPS and XR in parallel by applying +24V on both connectors UPS J108 & XR J203, if you will EPO them both at same time.

UPS can be configured in three other ways, concerning EPO. See UPS Installation manual for details. Battery XR frame can only be EPO by applying +24V on J203.

Schneider Electric Việt Nam

Phần đính kèm
XR EPO.pdf [327.09 KB]
Smart-UPS VT NAM Installation Single and parallel.pdf [6.1 MB]
Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: