What handles can be used with the GS2AH**F cable operator kits for GS2 Switches?

Issue:
Cable operator kit handle selection

Product Line:
GS2 fusible disconnect switches

Enviroment:
UL 98 IEC Style Disconnect Switches

Resolution:
These can use the 9422A1 to 9422A4 handles
NEMA type 1 3 3R 4 and 12 enclosures: 9422A3 (4 in handle depth) or 9422A1 (6 in handle depth)
NEMA type 4 and 4X stainless steel enclosures: 9422A4 (4 in handle depth) or 9422A2 (6 in handle depth)

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: