How many TCP connections does the Unity Momentum Ethernet port suppport?
Title
TCP connections supported by the Unity Momentum


Issue
TCP connections supported by the Unity Momentum

Product Line
Unity Momentum PLC

Environment
Unity

Cause
N/A

Resolution
The Unity Momentum Ethernet port can support 16 concurrent client connections and 16 concurrent Server connections.
Any PLC/SCADA sending a request to a Unity Momentum via Ethernet is connecting to one of the Unity Momentum Ethernet port's TCP Server connections.

If a Unity Momentum Ethernet port is issuing a ModbusTCP request to a remote node via a programmed MBP_MSTR blocks then that Unity momentum is using one of the TCP Client connections .

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: