What is the Stop and Go feature on the Altivar Process Drive?
Issue:
Stop and Go feature on the Altivar Process Drive

Product Line:
Altivar Process Drive

Environment:
All serial numbers for Altivar Process Drive

Cause:
N/A

Resolution:
The "Stop and Go“ function reduces the consumed energy when the motor is stopped and the power supply of the drive is switched on.

60% energy saving at stop (*)
Altivar Process switches off…
  • Power section (rectifier, DC-Bus)
  • Fans
  • Backlight of graphic keypad
Stop & Go control
  • Automatically when not running
  • Through communication network
  • Adjustable via a parameter
$0.00 additional investment
  • no line contactor required
  • no 24V external supply required

To Access
[My preferences] [Stop and go]

Key Notes:This function is available for drives from frame size 4 to 7. When the function is active, the DC bus voltage is no longer maintained at operational level in order to save energy.
When the drive is in energy saving state, the next run command shall be delayed up to 1 second during the DC bus charge.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: