How many expansion slots can be installed on the Altivar Process Drives?
Issue:
Expansion slots available with the Altivar Process Drives

Product Line:
Altivar Process Drives

Environment:
All serial numbers for Altivar Process Drives

Cause:
N/A

Resolution:
The Altivar 600/900 Process has 2 expansion slots:
  • Slot A (Right)
    • Legacy communication options
    • Advance Ethernet (only for ATV600)
    • IO Extension Module (VW3A3203)
    • IO Relays (VW3A3204)
  • Slot B (Left)
    • IO Extension Module (VW3A3203)
    • IO Relays (VW3A3204)
    • Encoder Module (only for ATV900)
  • Slot C (Top) - (VW3A3800 - Only for ATV900)
    • IO Extension Module (VW3A3203)
    • IO Relays (VW3A3204)
    • Safety option “premium” (VW3A3802)

Control electronic size does not change (even with 2 expansion cards used).
It is not possible to use the same expansion card twice and maximum one communication card is allowed.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: