A MES module is needed to read the status of the breaker and then the “circuit breaker control” function should be activated. Input I11 is used to monitor the open position while input I12 monitors the closed position. Then read the input via Modbus communication.
Đã phát hành cho:Schneider Electric Việt Nam