Will the M221 support the TM7 IP67 modules?

Issue:
Can the M221 controllers support the TM7 IP67 modules

Product Line:
All M221 Controllers

Environment:
Ecostruxure Machine Expert Basic ( formally  SoMachine Basic)

Resolution:
No. The TM7 modules are for the TM258 only. The M221 will support the ETB IP67.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: