UL Certificate of Conformity for Harmony HMIGTO series HMI
Issue
Where do I find the UL Certificate of Conformity for Harmony HMIGTO targets and which UL enclosure types are they rated for?

Product Line
Harmony HMIGTO

Environment
Physical characteristics

Resolution
Attached is the UL Certificate of Conformity for Harmony HMIGTO targets.

The HMIGTO series is was tested for UL Enclosure requirements:
Type 1, Type 4X (Indoor use only), and/or Type 13 rated enclosures

Schneider Electric Việt Nam

Phần đính kèm
CoC MPCKT-HMIGTO_20140318-E194434 (new UL File No. E220851).pdf [267.51 KB]
Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: