Video: How do I program an ATV320 to use the dial of drive as speed and Digital Input 1 (DI1) terminal as start and stop control?

Article available in these languages: Tiếng Phần Lan

Issue:
ATV320 to use the dial of drive as speed reference and Digital Input 1 (DI1) terminal as start/stop control

Product Line:
Altivar 320, ATV320

Environment:
All

Cause:
Programming setup

Resolution:



From Main Menu, press enter.
Scroll down to CONF and press enter.
Scroll down to FULL and press enter.
Scroll down to CTL and press enter.
Under CTL, set CHCF to SEP.
Set FR1 to A1U1.
Set CD1 to TER.

From the normal status display, press enter twice to then adjust the speed reference value as a % of the LSP-HSP range.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: