Will Quantum 140CPU65260 support X80 Ethernet Remote IO drops?
Issue
Does the 140CPU65260 support X80 Ethernet Remote IO drops

Product Line
Quantum, X80

Resolution
The Quantum 140CPU65260 does support the X80 Ethernet Remote IO drops. It supports both the BMxCRA312x0 and 140CRA31200 drops in the same configuration. Minimum required firmware version for 140CPU65260  is version 3.0.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: