Tìm các câu hỏi thường gặp
Does the ATV600 series drive have a multi-motor function?
Issue:
ATV600 series drive have a multi-motor function.
Product Line:
Altivar Process, ATV630, ATV650, ATV660, ATV680
Resolution:
ATV6xx does not have a multi-motor management function. The multi-motor feature is available in the ATV9xx series drive .
If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)
If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance:
Support | Schneider Electric Global (se.com)