KPI Calculation Engine Report
Issue
KPI Calculation Engine Report installation and configuration details

Product Line
​Power Monitoring Expert
PUE Summary Report
KPI Engine Calculation Report

Environment
Web Application Reports

Cause
PUE summary report calculations are incorrect in Power Monitoring Expert (PME)

Resolution
The KPI Calculation Engine Report requires a license to work with PME.
It is designed to operate on one or more  source\measurement pairs and perform a calculation based on a given expression to create a normalized data stream. The resultant values are presented in the report and can also be
optionally saved in the PME database against an output source\measurement.
See the attached for installation and configuration instructions.

Schneider Electric Việt Nam

Phần đính kèm
AZZO Calculation Engine.pdf [651.57 KB]
Tìm hiểu thêm
Phạm vi:
Sản phẩm:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi:
Sản phẩm: