How do you assign an IP address to a Connexium 499NOS17100 switch?
Title
Assign an IP address to a Connexium  499NOS17100

Issue
Assign an IP address to a Connexium  499NOS17100

Product Line
Connexium

Environment
Connexium

Cause
N/A

Resolution
To set the IP address, you will need to connect to the V24 port. See page 33.
Attached below is the manual for the 499NOS17100.

Schneider Electric Việt Nam

Phần đính kèm
499NOS17100_manual.zip [1.53 MB]
Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: