What is the ATV320's max frequency?

Article available in these languages: Czech

Issue:
Needs to know the ATV320's max frequency.

Product Line:
Altivar 320, ATV320

Environment:
All models

Cause:
N/A

Resolution:
The maximum frequency can be assigned to the tFr parameter in the drive's program, and tFr is adjustable between 10Hz and 599Hz.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: