Will an M340 processor run in an BMEXBPxx0x backplane?

Issue:
I mistakenly ordered a BMEXBP Backplane with my M340 CPU and X80 IO.
Will the M340 CPU still work with this backplane?

Product Line:
M340

Environment:
EcoStuxure Control Expert (formerly Unity Pro)

Resolution:
Yes. Although the BMEXBPxx0x backplane and the BMEXBPxx02 redundant backplane is designed for use with the M580 with the XBus and Ethernet Backplane, the M340 will operate normally in this backplane. The Ethernet side of the backplane will not be used.

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: