Video: Wiring & Programming Status Relays R1 & R2 on the ATV320 Drive

Article available in these languages: Tiếng Phần Lan

Issue:
How are the relays for ATV320 drive programmed?

Product Line:
Altivar 320

Cause:
Relay programming.

Resolution:
2 relays available: R1 and R2.
R1 can be wired as normally-open (R1A and R1C) or normally-closed (R1B and R1C).
R2 is normally-open only.

To program relays:
Enter and scroll down to CONF.
Enter and scroll down to FULL.
Enter and scroll down to I-O menu.
Enter and scroll down to R1- or R2- depending on preference.

See attachment for relay programming, relay delay time, relay active at, holding time, and relay fall back assignments.

Schneider Electric Việt Nam

Phần đính kèm

ATV320 relay programming.pdfATV320 relay programming.pdf [159.12 KB]
Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: