How to fix an unexpected shutdown of the Magelis iPC?
An important CPU usage brings about a temperature elevation of the CPU.
When the temperature threshold is reached, in order to safe the material, the operating system shuts down the system.

By default, this temperature threshold is set to 95°C but it is possible to increase it to 105°C.
See the procedure in the attached document.

iPC offer:
- Standard references: HMIBMPxxx, HMIBMUxxx, HMIPSPxxx, HMIPEPxxx, HMIPSOxxx
- Configured references: HMIPCCU2xxx, HMIPCCP2xxx, HMIPCCS2xxx

Schneider Electric Việt Nam

Phần đính kèm
CPU_Shutdown_Temeperature.pdf [310.32 KB]
Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: