Issue:
How does the Password protection set up in the ATV930 drive?
Product line:
ATV900, ATV930, ATV950, ATV960, Altivar Process
Environment:
All
Cause:
Firmware evolutions being worked on.
Resolution:
As of April 2017, Password is used to lock access for uploading or downloading a drive's configuration. This password will not lock menus or parameters in the keypad.
Evolution is planned for the further ATV900/ATV600/ATV340 versions in order to have password to protect the keypad access in addition to this parameter restricted access.
Đã phát hành cho:Schneider Electric Việt Nam