Where can you wire in a shutdown circuit on the ATV660 enclosed drives?
Issue:
Wire a shut down circuit on the ATV660 enclosed drives.

Product Line:
ATV660

Environment:
All

Cause:
Wants to wire in a Normally closed contact and shut down the drive if the contact opens.

Resolution:
You can remove the jumper between terminals 1 and 2 now you can wire in your normally closed contact between terminals 1 and 2.
Please note this is not your normal start and stop circuit. The normal start and stop for drive control is terminals 3 and 4.



Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: