Is the x80 I/O Class 1 Div 2 rated?
Issue:
Is the x80 I/O rated for hazardous locations?

Product Line:
x80 M340 M580

Resolution:
The Modicon x80 I/O is rated for hazardous location Class 1 Div 2 groups A,B,C,D in Canada and USA

82494_IMG

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: