Where can I get the cable pinouts for the Ethernet IP connector for the Altivar Process Drive?
Issue:
How can I get the cable pinouts for the Ethernet IP connector on the Altivar Process Drive?

Product Line:
Altivar Process Drive (ATV630, ATV930, ATV650, ATV950, ATV660, ATV960, ATV680, ATV980)

Environment:
All serial numbers, all model numbers

Cause:
Needs to know required cable connection pinouts

Resolution:

the cable pinouts for the Ethernet IP connector

Schneider Electric Việt Nam

Tìm hiểu thêm
Phạm vi:
Bài viết có thể hữu ích
Tìm hiểu thêm
Phạm vi: