Where do I find information on electrolyte contained within the SYBTU1-PLP and SYBTU2-PLP type APC, and/or the SE modular batteries such as GVSBTU, GVSBTHU and GVSBTHULL

Article available in these languages: Tiếng Tây Ban Nha

Issue:
Where to find information on electrolyte contained within the SYBTU1-PLP and SYBTU2-PLP type APC modular batteries, and/or the SE modular batteries such as GVSBTU, GVSBTHU and GVSBTHULL


Product line:
SYBTU1-PLP / SYBTU2-PLP, GVSBTU/GVSBTHU/GVSBTHULL


Environment:
PX1,2, 250-500, SUVT, Galaxy 3500, Galaxy VS


Information:
See application note 143 for specific values of contained electrolyte in both the SYBTU1-PLP (used in PX1 20,40, 48, 80 and 96KVA UPS units as well as the SUVT and Galaxy 3500 UPS units) and the SYBTU2-PLP (used in the PX2 100KVA and the PX 250/500KVA UPS units) batteries.

Application Note 143:
http://www.apc.com/salestools/SMCR-6NXGXU/SMCR-6NXGXU_R2_EN.pdf


Note – SYBTU1-PLP and SYBTU2-PLP use batteries manufactured by four different vendors. For further information on MSDS by the specific vendors please refer to FA157067

Also see FA157067

Galaxy VS Modular Batteries:
Battery TypeElectrolyte WeightElectrolyte Volume
(kg)(lbs)(ml)(gal)
GP1272F2FR0.51.113780.1
HR1234WF2FR0.440.983330.09
UP-PW1245P10.47941.0573780.0998
Battery TypeElectrolyte WeightElectrolyte Volume
(kg)(lbs)(ml)(gal)
GVSBTU511.137801
GVSBTHU4.49.833300.9
GVSBTHULL4.79410.5737800.998
Battery TypeElectrolyte WeightElectrolyte Volume
(kg)(lbs)(ml)(gal)
GVSBT42044.4151204
GVSBTH417.639.2133203.6
GVSBTH4LL19.17642.28151203.992

Schneider Electric Việt Nam

Phần đính kèm

Galaxy VS Modular Battery MSDS.pdfGalaxy VS Modular Battery MSDS.pdf [238 KB]
Tìm hiểu thêm
Phạm vi:
Tìm hiểu thêm
Phạm vi: